This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LXC2T45-Q1: The internal pull-down caused some circuits to malfunction

Part Number: SN74LXC2T45-Q1
Other Parts Discussed in Thread: SN74LVC2T45-Q1

Hi,

I have a customer design interface that needs a high level input, but SN74LXC2T45DCUR-Q1 was selected in the initial design without noticing that there was a pull-down resistor inside, so it cannot be used.

After that, CAVC2T45TDCURQ1, SN74LVC2T45QDCURQ1 and SN74AXC2T45QDCURQ1 without internal pulldown resistance were selected for testing, but the results were not OK.

So please help recommend this package P2P compatible, with a built-in pull-up chip, non-car gauge is also available.

Many thanks~

  • Hi Rhea,

    For LXC P2P please see the LVC family (SN74LVC2T45-Q1 for example).

    If additional help is needed, please help clarify what is meant by not okay results while also providing schematics and waveforms, thanks.

    Best Regards,

    Michael.