Part Number: SN74LV14A
We plan to change the constant of the damping resistance at the output destination on the current board.
As the output current increases, the peak current flows about 44 mA (1 μ or less) in a period of 10 to 20 μ.
(There is no problem at all with the actual and average values of about 10 mA even in the range that looks quite large.)
it can be read as 25mA continuous output and 50mA maximum output according to the data sheet. Is it OK to use a peak current of 44 mA in 10 to 20 μ cycles?