Part Number: SN74AVC4T774
Other Parts Discussed in Thread: SN74AXC4T774
Hi Sirs;
I need help for SN74AVC4T774RSV.
目前这个器件A port 是3.3V, B port是1.8V,但在使用过程中3.3V会比1.8V早上电。
当3.3V已经上电 1.8V 上电过程中,B2 信号会被传送到A2嘛?
我有做一个实验,在B2给了一个1.8V + 10k的上拉,同时捕获A2 和B2 的信号进行对比,其中A2 有发现一个L的波形,持续时间为35us,波形左端对应的B2电压为550mV左右(1.8V上电波形与B2相同),蛮疑惑这个波形的形成的?

thanks
zyong