This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC125: Product information for heat-resistant specifications of general purpose ICs and heat-resistant measures

Part Number: SN74HC125
Other Parts Discussed in Thread: SN74HCS125, SN74HCS541, SN74HCS138

お世話になります

弊社製品の温度特性検査にて御社のICを使ってます

汎用 (general purpose) IC 74HC125、74HC138、74HC541

温度範囲はマイナス40度からプラス90度です (temp range is -40 to +90 C)

数年でICの交換が必要となる為、対策として (as a countermeasure, the IC will need to be replaced in a few years)

耐熱仕様のICが無いか調査してます (investigating if there is an IC with heat-resistant specifications)

耐熱仕様があればご紹介ください (if you have heat-resistant specifications, let me know)

また槽内温度が高い場合の温度対策をご教示いただけるとありがたいです

よろしくお願いいたします