This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1T45: input levels above power levels (but below 5V)

Part Number: SN74LVC1T45


Is it possible to apply input signals to the SN74LVC1T45DRLR above the power levels not exceeding 5V?
I would like to power VCCA=VCCB=3.3V, so that the  VIHmin=2V because usually the inputs will receive 3.3V logic levels.
However my application requires the possibility to accept 5V logic levels as well.
Therefore, Is it safe to apply 5V input logic to the SN74LVC1T45DRLR with VCCA=VCCB=3.3V?