What is the input impedance, or input current, on the OE# pin of the SN74AHC1G125? The datasheet seems to imply this is a +/- 1uA, but the PSPICE model shows a 2000 ohm impedance to GND. Is this just an error in the spice model?
from the spice model...
.PARAM ROEZ = 2000
...
ROEZ OEZ GND {ROEZ}
I just wanted to make sure that this is actually high impedance (+/- 1uA) pin before I modify the spice model.
Thanks,
Eric