Part Number: TXB0106
Other Parts Discussed in Thread: PCA9535, TXU0304, TXU0104, TXU0204
HI
We are using the TXB0106 in unidirectional operation as shown in the document below.
VCCA is 1.8V and VCCB is 3.3V. The inputs, CELL($)_LT_1V8_VREG, are outputs from
individual 1.8V LD0's
We have changed the 10K series resistors (R196 through R200) to 1K and then to 22 Ohms.
At 1K the A($) input pins are at 1.65V and at 25Ohms they are at 1.8V.
I though the input load current was in the order of +/-2 uA max. It looks like we have around
150uA, given that we are dropping 0.15V across a 1K series resistor.
Am I misreading the datasheet? I also see that there is a requirement for the external drivers to have
drive capability of minimum of +/-2mA , which I assume is driving the gate capacitances and the
one shot logic on "transitions".
Is 22 ohm series resistance OK for this application or would you recommend a different value?
Regards
Finbarr