Part Number: SN74HCS273
Other Parts Discussed in Thread: UCC27517
Hi team,
My customer want to drive the gate of a FET by each output of SN74HCS273 directly. Their supply voltage is 3.3V.
The load(gate) capacitance is much higher than 50pF discribed in the datasheet for example 500pF~1000pF but, their operation frequency is very slow as 1kHz.
From dynamic power consumption point of view, it may be no problem because the operation frequency is low as 1kHz.
Pd = (Cpd * f * Vcc^2) + (Cl * f * Vcc^2 * 8bit) = 87.33uW
Is it okay that they connect a FET at each output of HCS273? Is there any other concern?
Best Regards,