Part Number: SN74LVC245A
I am using buffer SN74LVC245APWR (U5 in the attachment) with 3.3V as Vcc. When measuring the voltages on the I/O lines, I see a undershoot (on the incoming data to the buffer) going to -0.8V while the data sheet (section 7.1) says the minimum voltage applied on the I/O ports can be -0.5V. However the datasheet also says (in note (2)) that input/output negative voltage can be exceeded.
Can you please tell me if -0.8V on the incoming I/O ports can be accepted as an undershoot for this device without impacting the buffer's operation and reliability?
Please look at the attached document for more details.