Part Number: SN74LVC244A
Other Parts Discussed in Thread: SN74LVC16244A, SN74LVC245A, SN74AHCT244, TXU0204, TXU0102, TXU0101, TXU0304, TXU0104, TXU0202,
Hi,
Please see below queries and request you to suggest
Query1: Regarding 8 Bit Buffer IC SN74LVC244ARGYR , do you have similar one with 16 bit ?
TSSOP package is also fine in 16 bit i.e. Similar to 8 bit SN74LVC244APW
Query 2: Can you please suggest 8 bit bidirectional Buffer ICs whose inputs are tolerant to 5V or above ?
Please reply soon as possible.
Regards,
Puspam Nayak