Part Number: TXB0108
Other Parts Discussed in Thread: TXU0204, SN74LVC1G34
hello.
I intend to use the TXB0108 to translate my FPGA signals (1.8V) to/from several other components (3.3V)
My problem is as follows:
Most of these signal are 1:1, meaning one pin from the FPGA goes to one pin on a components. here I don't see any future problem.
However, 3 of there pins are 1:8. meaning of these pins will be connected to 8 components. In addition, these pins are only one direction (The "1" will always be output, and the "8" will always be input)
I was going to use one of the remainder pins of the TXB0108 to fan out to the 8 inputs, but now I'm thinking it may not work, and maybe I should either fan out to the TXB0108 (Instead of from the TXB0108, meaning FPGA pin to 8 different pins on the TXB0108) Or just use a different component, such as the TXU0204 or similiar.
Can you recomment me the next step?
Thank you.
Gady Wollmann