Part Number: TXH0137D-Q1
For TXH0137D-Q1, there are the following questions:
1. When will it be mass produced?
2. Please help provide the encapsulated AD file and send to my email yuhao-wang@ti.com thank you.
3. Help provide reference circuits
4. Is it possible to input a signal from A and give Y as an output to the MCU?
5. If VCC is connected to 12V according to 4, is it possible to damage the MCU pin connected to Y?