This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5V to 3.3 and vice versa



Basic idea is to connect mc68000 to cyclone II device, and to use that device to replace mc68000.

There is something wrong with quickswich devices. As I know MC68000 cant
support 3.3V (some versions can but mine just cant). When i use quickswich
any type i only get 5V to 3.3V translation and no vice versa. I need to use
dual voltage level translator with auto sensing. Only parts that I can
found with this is sn74lvc8t245(with direction control) and new one like txs0108e(no direction control).
For last two days I m reading about Pericom articles and those articles are
just like IDT have for quickswich part. Devices are working from higher to
lower and I m thinking that I just cant use those devices. For some devices
who work with 5V can drive lower voltage levels that is ok but on my
situation is not. For example PI5CX and PI3CX series are only related to 5V
to 3.3V translation no bidirectional and then i need to use bus enable
input like on most devices. From A to B bus or from B to A bus, that is not
practical. Also some Pericom devices PI74LVC4245 who have two voltage on
each bus side but no auto sensing again I need to set direction sides. I
just dont know, as much i m reading TI articles only thing is txs0108e that I m using
on design right now. Also using Pericom or IDT devices we can use pull up
resistor connected to higher power source. I just dont know....