This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4015B: Not getting the expected outputs for the given Clock and Data inputs

Part Number: CD4015B


Hello Everyone.

I'm using CD4015B Shift register in my design as shown in the attached image. Pin 9 is connected to 1MHz clock.  For data input, we are giving inverted signal of the Q4. 

We are expecting a 250kHz pulses in each outputs Q1, Q2, Q3 & Q4. But we dont see an expected outputs signals.

We are getting all outputs as 1V DC.

I have also connected 4.7K Pullup at the Data input pin and tried it (thinking at the initial point the input will be floating and hence I'm not getting the output). But still the outputs are same.

Can anyone please look at my design and help me if there are any problem in the design or suggest me what all I can do to rectify this issue.