Part Number: SN74AVC2T45
Other Parts Discussed in Thread: SN74AVC8T245
Hi Team,
We want to interface an eMMC 5.1 device [which supports a data rate of 400Mbps on each of its 8# data pins and has an IO voltage level of 1.8V] to an FPGA's GPIO pins [which supports 400Mbps on each GPIO pin and is having IO voltage level of 1.2V]. So, we need to use a level translator in between the FPGA and the eMMC device. Do you have any level translators that meet our requirement?