Part Number: SN74LVC1G123
Hello,
I need to generate an output pulse with a width between 1.2 and 1.5 seconds.
Looking at the SLA720a datasheet and application note, the maximum duration is obtained with a 200k resistor and a 1µF capacitor.
Can I increase the value of the resistor and capacitor to obtain a longer pulse duration?
I saw in the application note that as the capacitor increases, the K constant decreases. . Is possible to generate a 1.5 s pulse with this IC?
Best Regards.
Sylvain