Other Parts Discussed in Thread: SN74AXC8T245, TXV0108
Can I use the product with part number TXB0108 for CAN bus? When I look at the data rate of the material, it appears to be 100Mbps. Can bus is maximum speed 2Mbps. In this case, can I convert the processor outputs with 1.8V pins to 3.3V after connecting them to TXB0108 and then use them as can bus in the outside world with a high speed can transceiver? will I have problems with TXB0108 in this case?