This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G14: SN74LVC2G14 VT+ & VT- RANGE in VCC 3V

Part Number: SN74LVC2G14

Hi Expert,

I have a question about the material SN74LVC2G14.
Is the following understanding of the VT+ and VT- specifications in the following specification sheets correct?
Vcc=3V, VT voltage range 1.3~2.2V SN74LVC2G14 is judged as High
Vcc=3V, VT voltage range 0.6~1.3V SN74LVC2G14 is judged as Low
If so, then the following questions arise. Please help to confirm the reply.
1. High level=1.3~2.2V, what is above 2.2V?
2. Low level=0.6~1.3V, what is below 0.6V?
3. To avoid misjudgment of SN74LVC2G14, VT should try to give a low signal below 0.6V or a high signal above 2.2V?
4. How high frequency noise can the VT of this component detect? 100MHz? 250MHz?

Eddie

  • In the worst case, the input voltage must be above 2.2 V to be judged as high.
    In the worst case, the input voltage must be below 0.6 V to be judged as low.
    When the voltage is between 0.6 V and 2.2 V, the input state is not guaranteed.

    There is no guaranteed minimum input pulse width. If you want to ignore high-frequency noise, add a low-pass filter.

  • Hi Ladisch and Team,

    One question you loss is How high frequency noise can the VT of this component detect? 100MHz? 250MHz?

    Eddie

  • Hi,

    What do you mean by that question? The part can operate at a minimum frequency of ~180MHz at 3.3V VCC. I'm not sure what is meant by the voltage threshold detecting noise.

    Best,

    Malcolm

  • LVC can do at least 175 MHz in the worst case. The highest frequency it can actually detect in the 'best' case is much higher.

    In practice, you add a low-pass filter that removes all frequencies higher than those of your signals.