This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TXB0304's outputs have a lower impedance (1 kΩ instead of 4 kΩ). This means that the TXB0304 requires that the other devices have a higher drive strength, but it allows somewhat higher speeds. Only the TXB0104 supports 5 V.