Part Number: LSF0102
Hi experts,
Want to know the internal MOSFET architecture about LSF family. From training video said it is a four pin MOS, and from the illustration, base side connect to GND and Gate connect to Vbias.
1.Can you provide details of the internal MOSFET connect, construction and work status? The video is not very clear.
2.From data sheet and training video there is no transition waveform of DownStream(B drive A). Can you provide both Up/Down waveform? Due to LSF family is bi-direction LS, if the pass FET is connected as 3 pin NMOSFET, the transitions of UpStream and DownStream should be different.
Thanks