Part Number: TXS0102
Hello,
I would like to use the TXS0102 level shifter as selector via its OE input as described in the diagram below :

To read peripheral 1, OE_2, OE_3 and OE_4 are disabled and OE_1 is enabled and so on for other peripherals. Only one OE is high, the others must be low.
Is it possible to use the high impedance of each input/output when OE is low ?
Best regards
Jean-Francois