Part Number: TXU0304
Hi
This model is used at a temperature of 25° and a voltage of 3.3V. The chip output is abnormal and the failure ratio is 30%.
Could you please help confirm the cause
Thank you.



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXU0304
Hi
This model is used at a temperature of 25° and a voltage of 3.3V. The chip output is abnormal and the failure ratio is 30%.
Could you please help confirm the cause
Thank you.



I am not able to read the details on that screen. (Please note that your oscilloscope has a built-in screenshot function.)
But this looks as if some other device also drives the output. If there is no other output connected to the line, check for shorts.
Hi Yingjiao,
Please note that the feedback still holds i.e is this abnormal for all outputs or only a specific output? If so, ensure no bus contention where the output is also receiving an input. Also, check for shorts i.e known good unit vs suspected unit, thanks
Best Regards,
Michael.