This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
we use your TXB0104 for our new ODM project design,
our MCU control PSU(MCUoutput/PSU input) via TXB0104 level shift
(TXB0104 between MCU with PSU)
currently our customer highlight sometime power will be turn off randomly
we measure TXB0104 output pin (pin 7) get abnormally waveform as attached,
could you please give me some suggestion ?
Q1: why we see waveform will be switch ??
Q2: do you suggest pin to pin solution to replace defect parts??
[waveform]
[MCU TXB0104 circuit]
[PSU audio_on circuit]
The TXB has a drive strength of 20 µA, which is not enough for that circuit.
For unidirectional signals, use a unidirectional translator like the TXU0104/TXU0204/TXU0304.
Hi Clements
thanks for your reply, we will use TXU0104 to check , it drive strength up to 12mA at 5V,
because I need to explain why work abnormally with my customer, I can't find driver strength of 『20uA』 in datasheet ,
could you tell me where I can find it.
Hi David,
Please help see below from the datasheet, thanks.
Best Regards,
Michael.