This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108PWR - 8 channel Level translator



Hi,

 

                 We are using the Part No:TXB0108PWR - 8 channel Level  translator. Connected VCCA to 3.3V, VCCB to 5V,OE - 3.3V . We are using first two (1&2)channels for transferring the Clk signal 18.432MHz from A port to B port. We are not getting the 5V level shifted output at the B port. Instead we are getting 3.14V clock output. The Translator is not shifting the Logic output from 3.3V to 5V. The input to level shifter is 3.3V ,18.432MHZ signal.

 

                We probed the signal at both A port and B port. The Clk  Voltage is  measured at A port is 3.4V,18.432MHz. But,the Clk  Voltage is  measured at B port is 3.2V,18.432MHz.

The voltage level is getting dropped instead of getting level shifted to 5V.

 

We need suggestions to solve this problem.