Other Parts Discussed in Thread: SN74AXC4T774, TXU0304, TXU0104, TXU0204, TXB0304
This is a question for both the AVX and the AVC parts.
- We are having the VCCA coming up first and the VCCB coming up after a few seconds. In the meantime, the direction pins are pulled low and high to set the direction.
- The OE is pulled low from power on VCC_A.
- We are seeing a high current being taken on the VCCA during this time. VCCB is a floating voltage around 0.6Volts in these initial few seconds.
- If we ensure that the OE is pulled high for the time till VCCB is not present and then comes down low, will we see this high current draw again due to a floating input on the B side,
- Or will the OE enable high take care of isolating the input on the B side till the OE is pulled low?