Part Number: SN7406
Other Parts Discussed in Thread: SN74LS06, SN74LVC1G07,
Hi,
There are more than 2 devices that share (over the cable) same bus. Each bus line is pulled high to 5V over 1k resistor, and for low value is used 7406. I am adding new device to the same bus. Can I use sn74ls06 instead of non ls device? I checked datasheet and both (ls and non ls) have almost the same switching characteristics. On device input is 3.3V signal from microcontroller pin (few mA) and device output is connected to bus (over the cable).
Regards,
JH