Part Number: SN74LVC00A
Other Parts Discussed in Thread: SN74LVC3G17, SN74LVC07A
Hi,
if you can help with this customer query?
The TI data sheet for both 74LVC14 and 74LVC00 suggest the recommended Vcc maximum is 3.6 volts, but the absolute max is shown at 6.5 volts. If the Ab max really is 6.5 volts, then why can’t these be used with 5V Vcc? – would there be a reliability issue running at 5v Vcc given this is significantly lower than ab max?
Thanks,
Jani