Other Parts Discussed in Thread: TXU0101, SN74LXC1T45
Hi Team,
My customer are using LT +LOGIC GATES packaged parts for gated+ level shifting
their input logics are in 1.8V and 3.3V o/p logic has to be in 5v
They provided 5v VCC for the supply
Since one of their input is 1.8V it will violate VIH min req
Can you please help to check if there are parts that supports for 1.8V logic levels as well with (low delay <15 ns ) ?

I search the below parts but all of them has a VIH more than 2V
SN74LV1T32DBVRG4,SN74LV1T08DBVR,SN74LV1T00DBVR
Please advise. Thanks!