Hello,
I'm looking to use the TXU0304 for level shifting from 1.8V -> 1.2V. The datasheet says it can support 10 mbps Min over the temperature range (Table 7.6). I'm wondering if you have a graph that specifies this MIN value for the max data rate from 1.8V -> 1.2V across the temperature range?
If not, what is the MIN value for the max data rate at 20°C for 1.8V -> 1.2V level translation?