Part Number: TXS0102
Other Parts Discussed in Thread: PCA9306, LSF0102
Connecting CPU (PIC) and TXS0102.
I have the following waveform, is there any solution?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TXS has edge accelerators to allow high data rates. Apparently, your bus capacitance is so high that the accelerator cannot (dis)charge it completely.
Where did you measure these spikes? Are they visible only at the TXS pins, or also at the I²C devices?
I²C is a slow protocol and does not need edge accelerators. You could use a simpler translator like the LSF0102/PCA9306.
Hey Shinji,
Similar to what Clemens' mentioned, this is a side effect of using the TXS0102 to drive signals across long cabling/ PCB traces. The TXS0102 uses one shot circuitry to speed up the rise times, but if the output capacitive load is too high, the one shot can time out prematurely as we see here.
You may also see Leveraging Edge Rate Accelerators with Auto-Sensing Level Shifters for further clarification.
Regards,
Jack
Thank you for answering.
Also slightly observed on I²C devices.
Please tell me the difference between LSF0102/PCA9306 that you introduced.
Which one is suitable?