Hi,
I try to use a SN74LV1T125DBVR in my design as an interface between a 3.3V CMOS device and a 5V TTL device.
I use it like this :
Input A > pin 2 > GPIO Signal 0V or 3.3V
Ouput Y > pin 4 > GPIO Signal 0V or 5V
VCC > pin 5 > VCC = 5Vdc with 100nF Ceramic capacitor
GND > pin 3 > GND
OE > pin 1 > to GND
When I use the devoce like this It doesn't work ?

Have you an idea please ?
Thanks