This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: I2C communication using TXS0108E

Part Number: TXS0108E

I have a question about the TXS0108E 8-Bit Bi-directional, Level-Shifting, Voltage Translator.
In our circuit, we use TXS0108E for the I2C communication line to change the level, but depending on the pull-up resistor value, abnormal oscillation will occur in the signal.
(See file: 20240325_Circuit_and_waveform.jpg)
(1).The TXS0108E is said to switch the direction of the signal automatically, but I am looking for documentation explaining its operation.
Will the port side where the voltage changes (L→H or H→L) be judged as the input port and the other side will be switched to the output port?
(2).What are the possible causes of oscillation? 
  • The TXS does not really detect the direction; the circuits on both sides are always active.

    Oscillations are usually caused by ringing that is amplified by the TXS's edge accelerators. Do you have long traces, connectors, or cables?

  • Hey Yamamotoju,

    External pullups are no longer needed for this device and can be removed since the TXS translators have internal 10kohm pullups. 

    1. The device is open-drain based.  For any input signals lower then VCC, the low signal will be propagated to the output as logic low with the internal switch acting as a resistor. Similarly for input signals near VCC, the switch will be open and a high state is achieved on the outputs. One shot circuitry is also included to provide faster transition times during a L-> H and H-> L. You can see more on its operation here in this app note: A Guide to Voltage Translation With TXS-Type Translators

    2. It could be the one shot circuitry being retriggered by accident. Please ensure proper ground connections and the output cap. loading is kept to a minimum. 


    Regards,

    Jack 

  • I delayed to reply.
    >Oscillations are usually caused by ringing that is amplified by the TXS's edge accelerator. Do you have long traces, connectors, or cables?
    ⇒Are there any length regulations? (For example, 200mm or less...etc.)
    In this experiment, we were able to reproduce the oscillation phenomenon, but when the pull-up resistance value on the CPU side becomes low, the oscillation phenomenon occurs.
    When the VIL on the A port side increases and the VOL on the B port side exceeds 0.15V, the original B→A signal transmission repeats B→A→B→A... I think that a one-shot circuit is working, but is such behavior possible?

  • Hi Yamamotoju,

    Yes, please see  Leveraging Edge Rate Accelerators with Auto-Sensing Level Shifters mentioning about 64 mm dependent on your design factors.

    Also, yes pull-ups impacts the switching levels, with the referenced app note further clarify your concerns, thanks.

    Best Regards,

    Michael.