This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC04: SN74HC04DR Performance problem

Part Number: SN74HC04

Hi

We have tested this product and found that the waveform is inconsistent, but the results of our two different screen printing tests are inconsistent. The screen printing of TI is normal, while the screen printing of printing is bad

Could you please help confirm the cause

thank you.

  • Both markings look valid 

    I do not understand your description. What are the input and output waveforms? I do not see a valid logic signal anywhere.

  • Hello, could you please help to confirm whether the power consumption of goods of Chinese origin is the same as that of goods of Mexican origin? Everything is normal when we use goods of Mexican origin, but abnormal when we use goods of Chinese origin, abnormal situation: the output voltage is pulled down by about 50%

  • There are different dies that can have different behaviours when you violate the recommended operating conditions, especially VIH, VIL, or ∆v/∆t. I suspect this is the case here. Please show the schematic of the test circuit, and specify exactly which waveforms are input and output signals.