This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a question about the TXS0108E 8-Bit Bi-directional, Level-Shifting, Voltage Translator.
The unused terminals in our circuit are connected to GND through a 10kΩ resistor at both ends of the A and B ports.
How to deal with searching for "E2E" "[FAQ] What should be done with unused I/O pins of the level translator devices?"
]
e2e.ti.com/.../faq-what-should-be-done-with-unused-i-o-pins-of-the-level- translator-devices
According to the TXS series, it can be interpreted as unconnected.
Also, "For TXS devices, the internal 10kohm pull-ups..." in the text applies to the TXS series TXS0101, TXS0102, TXS0104, and the TXS0108E we are using has an "H" level instead of an internal 10kΩ. The 4kΩ "L" level is written as 40kΩ, so I think it's strictly different.
What I want to check is
(1).Could you please tell me how to dispose of unused terminals in the case of the correct TXS0108E?
(2).Please let me know if there are any negative effects with the current connection of our circuit (connecting both ends of unused terminals to GND via 10kΩ).
1. All TXS devices have internal pull-ups and should never be used with external pull-downs, whether used or unused. Unused pins should be left open.
2. The internal and external resistors form a voltage divider; the exact voltage depends on whether you end up with 4 kΩ or 40 kΩ. The only negative effect is increased power consumption.