Part Number: SN74LVCH8T245
HI sir
I saw the thermal pad connect to PIN 21, But the PIN 21 is the B1, Please advise it,thanks



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVCH8T245
HI sir
I saw the thermal pad connect to PIN 21, But the PIN 21 is the B1, Please advise it,thanks



This is an error; the pad is pin 25. (This is correct in the board layout and stencil design on the next two pages.) It is considered a pin separate from all others.
In logic devices, the pad is connected to GND. But this is an internal connection (like pins 12 and 13) that has no influence on pin numbers.