Hi.
I have a question about output enable control of TXU0204.
My design is like below.
- VCCA=3.3V(Fixed), VCCB= 1.8V or 3.3V(Default)
- Output Enable referenced to VCCA through 10kohm resistor
From the link below Karan mentioned that powering VccB off while INA is in a high state.
What if output enable pin is in low state and then VccB is powered off while INA is in a high state? Would it be either undesirable situation?
Regards.