Part Number: LSF0102
Other Parts Discussed in Thread: TCA39306,
Hi
Could you help recommend a Level translator that can be used below 50MHz and can be used to convert 3.3V to 1V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
A wide range of the translator portfolio can be used to support the above conditions. Please see Voltage Translation Application Quick Reference for general recs depending on the interface of your signals. Is there a specific direction of the signals per ch., ch. count or timing requirements?
Regards,
Jack
Hey Gareth,
In addition to Clemens' question, please also reference Voltage-Level Translation With the LSF Family for additional careabouts when designing with the device.
Regards,
Jack