Other Parts Discussed in Thread: SN74LVC1G3157, TS5A63157, SN74LVC2G53
Hi,
We are using SN74AXCH8T245PWR in our design to convert 25MHz signal from 3.3V to 0.75V. When we got the board and test it, we see that this part is not supporting 25MHz at these voltages and only supporting till 5MHz. Request you to let us know about possible solution to mitigate this issue.
We see that if we change the lower side voltage from 0.75V to 1V, it is working fine. But it is not an option for us.
Is there any alternate device or planned device to support this requirement, please suggest.
Regards
Sharath Chandra