Please share the Maximum junction temperature (Tjmax) and ESD details for this part
CD4555BPWR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Anitha,
The temperature specs for this part are below
| Theta JA-High K | 105.3 |
| Theta JC, top | 40.1 |
| Theta JB | 50.3 |
| Psi JT | 3.4 |
| Psi JB | 49.8 |
We do not have ESD specs for this part are
ESD-CDM 1000 V
ESD-HBM 2000 V
Regards,
Owen