This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G32-Q1: IF the OR IC power supply is 1.8V,the input high can be 3.3V signal?

Part Number: SN74LVC1G32-Q1

Hi,

In my design, I want to design a OR circuit, I have a problem:

if the OR IC power supply is 1.8V, so that the output high is 1.8V, but the input is 3.3V voltage, is the input OK?

Thanks,

Kai