Other Parts Discussed in Thread: LSF0101
Hi Team,
I am using SN74AXC1T45DBVR in design.
I am converting VCCA= 1V to VCCB= 1.8V
VOH min is 0.6V of Master device
VIH min of SN74 is 0.7V at 1V(VCCI).
Do you think there will any issue in communication with Master?
Can you suggest 1 bit level translator which have Vih min 0.5V.
Many Thanks
Rajat