This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G17: Electrical characteristics difference between packages

Part Number: SN74LVC1G17


Hello experts,

I had a quick question, between SN74LVC1G17DBVR [SOT-23] and SN74LVC1G17DCKR[SC70], are there any differences between them other than package type, spec-wise?

Customer asked this and my understanding is that the electrical characteristics & IC spec is the same for both packages, except for thermal. I just wanted to double check.

Thank you.

  • There are indeed very small differences, as shown in the IBIS model:

    |******************************************************************************
    | Component LVC1G17_DCK 5-pin SOT
    |******************************************************************************
    |
    [Component]            LVC1G17_DCK
    [Manufacturer]         Texas Instruments, Inc.
    [Package]
    |                                           typ         min         max
    R_pkg                                       2.000e-02   1.700e-02   2.500e-02
    L_pkg                                       9.980e-10   8.810e-10   1.069e-09
    C_pkg                                       1.460e-13   1.180e-13   2.050e-13
    |
    |******************************************************************************
    |
    [Pin]    signal_name   model_name           R_pin       L_pin       C_pin
    |
    1           nc         nc                   1.900e-02   1.069e-09   1.620e-13
    2           A          LVC1G17_IN           1.800e-02   8.810e-10   1.210e-13
    3           GND        GND                  1.700e-02   1.031e-09   2.050e-13
    4           Y          LVC1G17_OUT          2.000e-02   9.600e-10   1.240e-13
    5           VCC        POWER                2.500e-02   1.049e-09   1.180e-13
    |
    |******************************************************************************
    | Component LVC1G17_DBV 5-pin SOT
    |******************************************************************************
    |
    [Component]            LVC1G17_DBV
    [Manufacturer]         Texas Instruments, Inc.
    [Package]
    |                                           typ         min         max
    R_pkg                                       2.500e-02   2.100e-02   2.900e-02
    L_pkg                                       1.529e-09   1.312e-09   1.906e-09
    C_pkg                                       1.560e-13   1.100e-13   2.400e-13
    |
    |******************************************************************************
    |
    [Pin]    signal_name   model_name           R_pin       L_pin       C_pin
    |
    1           nc         nc                   2.100e-02   1.511e-09   1.440e-13
    2           A          LVC1G17_IN           2.300e-02   1.312e-09   1.380e-13
    3           GND        GND                  2.900e-02   1.906e-09   2.400e-13
    4           Y          LVC1G17_OUT          2.600e-02   1.541e-09   1.500e-13
    5           VCC        POWER                2.500e-02   1.374e-09   1.100e-13

    However, the guaranteed electrical characteristics in sections 6.5…6.9 are the same for all packages, and the difference in the typical characteristics is so small that it is negligible.