Hello everyone.
I am trying to run the bldc motors of an old cnc using step and direction pulses.
Everything works fine, but I have a loss of step signal.
I use an arduino uno with Estlcam to generate the pulses
, I have mounted a 5v to 3.3v converter (txs0108E) on this one to send the pulses to the stm32f446 and IHM07M1 driver assembly.
Capturing the signal I have realized that the High Voltage level (3V) output of the converter is just over 2V (2.09v). If I don’t connect the output to the stm board it is 3V.
I don’t know if putting a pull up resistor at the output would be a good idea.
What do you recommend?
Thanks