Other Parts Discussed in Thread: LSF0002
Hi Support
I want a part for IO level shifting between 1.2V and 1.8V. IO could be push-pull or open-drain. And I want auto bi-direction.
I found LSF0102 may fulfill the requirement. And I come across one application report called "Voltage-Level Translation With the LSF Family"
Quote: The data sheet says Vref_B must be 0.8 V higher than Vref_A. How do I translate across a small range, like 1.2 V to 1.8 V?
It says : Set Vref_A to 1.2 V and Vref_B between 2 V and 5.5 V. Add a B-side pullup to 1.8 V. As long as Vref_B ≥
Vref_A + 0.8 V and Vref_B is within the recommended operating conditions range, the level of Vref_B
does not affect the output signal. Only the B-side pullups affect the output signal level.
Could you please help to explain more how to connect it correctly or review my circuit if I connect it right?