Part Number: TXU0304
Other Parts Discussed in Thread: SN74LVC125A, SN74LVC244A
Hi,
I need to use SPI master/slave configuration, have one STM32 as master uC as SPI master & 6 STM32 are slaves, i was trying on one prototype which involved external wiring, bus without repeater, facing issues in SPI communication, it can work for lower frequency less than 400kHZ, then i thought to use bus repeater, if I use TXU0304 for all 4 signals(MISO/MOSI/CS/CLK),which way is correct, one TXU0304 is for one slave(means total 6 TXU0304- input is common & output is dedicated to each slave) or I can use only one TXU0304 for all 6 slaves, Please advice which is the best methodology.
Thankyou.
Manmohan