Part Number: TXV0106
In addition to the error with the diagram on the first page of the datasheet, we have also found the following potential sources of confusion:
1. Figure 7-1 Functional Block Diagram of the TXV0106 shows an active high OE pin, as well as two internal invertors, the Output Enable should be active low right?

2. Table 7-1 Series Resistor Values for 50ohm Impedance Matching shows a 53ohm resistor for a 1V2 output voltage, this looks to be incorrect if you consider the resistor values given for the other output voltages 1V8, 2V5 and 3V3. Can you confirm the resistor value required for a 1V2 output?

Thanks in advance
Nick