This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LXC2T45: SN74LXC2T45

Part Number: SN74LXC2T45
Other Parts Discussed in Thread: SN74LXC1T45

Good morning

Can you kindly suggest the Level shifter for the below mentioned Requirements

 

  • Output current – 32mA max
  • Non-isolation
  • Communication Procedure - Start-stop synchronous (Asynchronous)
  • Communication speed - 38.4kbps
  • How to Transmit - Full duplex
  • Date length – 8bit
  • Stop bit length – 1bit
  • Parity - No parity
  • Transmission Code – binary
  • Error detecting - Framing, Overrun
  • Communication Cycle – 6ms
  • Output current – 32mA max

Thanks, and Regards

Nithya N