Question 1 :
The Absolute Maximum Ratings shows Vo=Vcc+0.7V (Max)
It's means 7V+0.7V? or Vcc is typical use Vcc? (ex If use Vcc=3.3V, Vo=3.3+0.7?)
Question 2 :
The Recommended Operating Conditions shows Vo=5.5V (Max)
It's means in any condition, as long as it is less than 5.5v?
(Even Vcc=3.3V, but pullup resistor to 5V)


Question3 :
Can I design the circuit below (Vcc=3.3V, but pullup resistor to 5V)?

There are two ways to explain
1. Vcc=3.3V, then VOH=5V <The Recommended Operating Conditions shows Vo=5.5V (Max).-->OK
2. Vcc=3.3V, then VOH=5V > The Absolute Maximum Ratings shows Vo=Vcc+0.7V=3.3+0.7=4V-->NG