Part Number: TXS0102-Q1
Other Parts Discussed in Thread: LSF0102, LSF0002, TXS0102,
Dear,
We are using TXS0102DCUR (main source) and TXS0102QDCURQ1 (second source) at our mass production project. Now we meet an unexpected issue:
Issue phenomenon:
We capture some fail waveforms at the same board, using TXS0102DCUR VS TXS0102QDCURQ1. From the failed waveform, we suppose it triggers one-shot feature.
It confuses us: there is only one pulse when using TXS0102DCUR, but there are 3 pulses when using TXS0102QDCURQ1? We want to know which parameter of TXS0102DCUR or TXS0102QDCURQ1 causes the difference: one pulse or three pulses.
Q1:
About the one-shot feature, what are the main differences between TXS0102DCUR and TXS0102QDCURQ1? What are the Vt (trigger one-shot threshold voltage) of TXS0102DCUR VS TXS0102QDCURQ1.
which will trigger one-shot more easily?
Q2:
How wide are the pulse durations of TXS0102DCUR and TXS0102QDCURQ1, when trigger one-shot feature?
Q3:
Why are the number of pulse waveforms different at the same board? One pulse when using TXS0102DCUR, while three pulse when using TXS0102QDCURQ1。
Q4:
The operation temperature of TXS0102DCUR is -40°C~85°C, it is Industrial grade? The datasheet didn't say it is Industrial grade. Our customer wants to know whether TXS0102DCUR is industrial grade or not.
TXS0102QDCURQ1 meet three abnormal pulses:

TXS0102DCUR meet an abnormal pulse:

waveform test point: