Part Number: TXB0302
Circuit has a test mode where both sides of TXB0302 are tri-stated. 20K+ pullup on 3.3V side, 25K + pulldown on 2.5V side. 2nd data path has 40K and 20K pullups. I presume the output state of the TB0302 is indeterminate since none of the cases meet the sink/source requirements to force device to known state, which is OK in this mode. It appears these use cases will cause increased power dissipation within the IC. Is this continuous current / dissipation enough to cause damage to the device(output driver), assuming office ambient temperatures?